AXIS#.SENSORLESS.FAULTTIME

Description

In Sensorless Field-Oriented Control (SFOC), if the estimated commutation angle error goes above AXIS#.SENSORLESS​.FAULTANGLE for at least AXIS#.SENSORLESS.FAULTTIME, a fault is detected. Adjust these two values as needed.

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type

Read/Write

Description Sets the minimum fault detection time for SFOC

Units

ms

Range 1 to 10000
Default Value 10

Data Type

Float
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
AXIS1.SENSORLESS.FAULTTIME

5018h

04h

Signed32

-

1000:1

Read/Write

No

AXIS2.SENSORLESS.FAULTTIME

5118h

04h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SENSORLESS.FAULTTIME

7403

1CEB

Signed32

Read/Write

-

AXIS2.SENSORLESS.FAULTTIME

72939

11CE

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SENSORLESS.FAULTTIME

7403

Float

Read/Write

-